From Diagnostic List - Any of the compressor's motor winding temperature sensors is seen to be beyond the winding rated temperature of 265°F (129.4°C).
To confirm that there is a faulty motor winding temperature sensor; we recommend you obtain a Chiller Service Report, DataRecorder Files, Default File, Datalog File. Review the files to confirm temperatures exceed the trip point listed above. Determine if the issue is just a faulty sensor, two sensors, wiring, connections, or failed compressor.
- If a failed compressor is confirmed, leading to this diagnostic...replace the compressor.
- If there are wiring issues, correct the wiring.
- If there is a sensor issue; reading incorrectly, and ALL of the other sensors are reading correctly, there are options to take:
- Disconnect the failed sensor and place an external 110.0 Ω ½-watt resistor across the Wind Temperature Sensor LLID Input. You will still have other sensor working; and the resistor will ensure the control system is satisfied.
- Disconnect the faulty sensor and change the following settings in the chiller using Tracer TU
- UC800 Controls: While connected to the chiller with Tracer TU, proceed to the Utilities tab, then follow the dropdown menus to Equipment \ Field Startup \ Features Settings Circuit xx.
- Symbio800 Controls: the setting can be found in Level 4 Gains and Start Sequence
- Default setting is Warning
Change from Warning to NONE
Additional details
Notes
- High Motor Winding Temperature
- High Motor Winding Temperature - Cprsr1A
- High Motor Winding Temperature - Cprsr2A
- There is not a field provided method to physically replace a Winding Temperature Sensor in a GP4 compressor. ( It is physically impossible to embed a new sensor in the motor windings. )
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.