Can I convert the RTAF from R134a to R513A?
Replacing R134a with R513A is a relatively easy process.
- What parts need to be changed out?
- Just refrigerant
- Different lubricant / oil?
- Same oil
- Does the refrigerant system need to be cleaned/flushed before putting new oil and R513A refrigerant?
- No, R513A is compatible with R134a
- Do we have a UC800 “flash” for R513A, or does the Trane technician have to manually change the settings/safeties?
- Yes, the controls configuration will need to be updated to show R513A – slightly different properties and control algorithms.
Additional details
Other Question/Problem/Cause Statements
- What is necessary to convert an RTAF charged with R134a to R513A?
- Can this chiller be converted to R513A?
- Is RTAF convertible and compatible with R513A refrigerant?
Facts
- Air-Cooled Chiller (Pueblo) (RTAF)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.