Phase reversal diagnostic
- If Phase Reversal protection is active; the controls will not let the compressor attempt to spin the rotors.
- If you hear the compressor actually starting, the real problem is likely to be Phase Loss.
- However, the Phase Rotation circuitry is responsible for Phase Loss prior to the starter transition. I suspect the real diagnostic is Phase Loss which is being called out by the Phase Reversal Protection circuitry prior to transition.
See RLC-SVB15A-EN for reference and cause resolution.
Additional details
Other Question/Problem/Cause Statements
- Phase reversal diagnostic
- Phase Loss diagnostic
Facts
- Chiller is attempting to start. The chiller is turning over; the rotors are spinning.
- Diagnostic prior to transition; but after compressor rotors are spinning.
- Water-Cooled Chiller (Pueblo) (RTHB)
- Water-Cooled Chiller (Pueblo) (RTHC)
- Water-Cooled Chiller (Pueblo) (RTHD)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.