UCP2
Diagnostic: Transition Complete Input Shorted
- Source: Starter
- Active Period: Starting Compressor
- Severity: Immediate Shutdown
- Persistence: Latching
- Description of Trigger Behavior: The Transition Complete input was found to be shorted before the compressor was started.
Troubleshooting Guide:
- This diagnostic is active for all electromechanical starters.
- Verify the Opto Input J4-2 does not have 120VAC on it prior to start.
- Verify the AUX contacts that supply the 120VAC to to J4-2 are not faulty.
- Verify the Opto Input J4-1 Neutral in correct and electrically connected.
Notes
- See appropriate IOM for reference.
Additional details
Other Question/Problem/Cause Statements
- Transition Complete input shorted
Facts
- UCP2
- Water-Cooled Chiller (Pueblo) (RTHB)
- Water-Cooled Chiller (Pueblo) (RTHC)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.