RTHB
- Check the voltage on the 2U1 Starter Module, J4-2.
- It is possible that the 2K2 Auxiliary contactor is leaking current (not fully open) and is energizing the opto input in the module.
- There should be zero voltage at J4-2 when the Run contactor is de-energized.
- If there is a voltage present, disconnect the input voltage to auxiliary contactor and check for voltage again.
- If the measured voltage is zero with the contactor disconnected, replace the contactor.
Additional details
Other Question/Problem/Cause Statements
- The Transition complete input was found to be shorted before the compressor was started
Facts
- RTHB
- Water-Cooled Chiller (Pueblo) (RTHB)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.