RTHC:
- Remove line voltage.
- Remove ground connection at 1TB3-1 to isolate ground(s).
- You may need to remove 1F1-1F3 also, when doing this test.
- Apply an external 115VAC to 1TB3-10 (hot) to 1TB3-1 (neutral).
- Once control power is applied to the micro, disable the under/over voltage protection.
- Starter Dry Run is initiated in the "Service Test" group. This group is password protected (++--++, Enter).
- Step through the service test group to starter dry run and initiate the test.
Notes
- For additional Starter dry run timing requirements, see Diagnostic and Controls Troubleshooting RTHC-SVD01B-EN. For alternate procedure, refer to page 45 of this bulletin, a 24 VAC transformer will be needed.
Additional details
Other Question/Problem/Cause Statements
- Starter dry run
- Test run the starter
- Starter dry run test
Facts
- Water-Cooled Chiller (Pueblo) (RTHC)
- UCP2 Dry Run
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.