RTAA 70-125 TON Chiller, RTCA 70-125 TON Condenser:
- Pre-Revcor Fans (October 2006): The Low ambient option for RTAA/RTCA Chiller/Condenser used variable frequency drives (VFD's) tied in to the lead fan of each circuit.
- When a chiller/condenser is purchased without the low ambient option, the chiller will come standard with a 1/2 pitch 3-blade fan on the lead fan motor for each circuit.
- Therefore, under the Service Settings Menu, "variable speed fan, circuit 1 & 2" should be set to Disable and "Low Ambient Unit, Half Airflow Fan" should be set to Enable.
Additional details
Other Question/Problem/Cause Statements
- RTAA/RTCA Air Cooled chillers without low ambient option?
- What are the fan configurations on 70-125 ton Chillers/Condensers?
Facts
- Air-Cooled Chiller (Pueblo) (RTAA 70-125 Ton)
- Air-Cooled Condenser (Pueblo) (RTCA)
- Compressor Chiller (Pueblo) (RTUA)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.