Field installing the low ambient option
- To add the low ambient option (variable speed drives, VFD's) according to the wiring diagram in the installation operation manual, it is necessary to introduce the 1U3 module to the main processor (Dynaview) using the binding process.
- First, the chiller configuration must be done using the Techview Service Tool.
- Establish a local connection to the display, access the Configuration View screen, and select the Feature Tab.
- Scroll down to CDTY (Condenser Temp Range) and choose L-Low Ambient Capability Condenser.
- Load this configuration at the bottom of the menu.
- Once the loading is complete, the display will enter the Binding View Menu.
- The 1U3, 1U15, and 1U20 modules must be bound to enable the low ambient option.
- Finally, access the Setpoint View and scroll down to the last item, Freeze Avoidance Start Inhibit.
- Disable this feature to allow the chiller to operate below 25F ambient temperature.
- If this feature is not disabled, the chiller will shut down in a Start Inhibit by Cold Condenser Temperature operating mode.
Additional details
Facts
- Air-Cooled Chiller (Pueblo) (RTAC)
- 1U3 module (Dual Inverter Interface, Fan Speed Command and Fault Feedback) installed
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.