Chiller is not loading up fast enough; how can I get the chiller to load quicker?
RTWA 70-125, RTAA 70-125, RTUA 70-125 TON chillers:
- This chiller utilizes PID control.
- Within the Service Settings Menu of this control platform, there is a specific parameter referred to as "Leaving Water Temperature Control Response Setpoint".
- By default, this parameter is set to 40, with a configurable range of 2 to 200.
- To accelerate the loading process of the chiller, it is advisable to raise the value of this parameter.
Conversely, if the intention is to decelerate the chiller's loading speed, it is recommended to decrease the value of this parameter.
Additional details
Other Question/Problem/Cause Statements
- Chiller is not loading up fast enough; how can I get the chiller to load quicker?
- Chilled water control response.
- How could I get the chiller not to load as fast?
Facts
- Air-Cooled Chiller (Pueblo) (RTAA 70-125 Ton)
- Compressor Chiller (Pueblo) (RTUA)
- Water-Cooled Chiller (Pueblo) (RTWA)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.