RTAA 70-125 Ton, RTWA 70-125 Ton, RTUA 70-125 Ton Chillers:
- These fuses provide line voltage/power to the 120VAC Control Power Transformer (Step-down Transformer)
- These fuses ALSO provide voltage to the Under/Over Voltage Transformer.
- Under Voltage issue:
- The Under/Over Voltage feature can be disabled.
- The wiring going to the 1T2 Transformer can be disconnected.
- Please refer to the Transformer Checkout Procedure in the Controls Troubleshooting Bulletin (RLC-SVD03A-EN — attached at bottom of article) and replace the 1T2 if needed.
Additional details
Other Question/Problem/Cause Statements
- 1F16 and 1F17 fuses are blowing
- Loss of 120VAC Control Power
- Under Voltage
- No voltage display on Human Interface
Facts
- Air-Cooled Chiller (Pueblo) (RTAA 70-125 Ton)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.