Can I do a service pumpdown and store the refrigerant in the condenser?
RTAC Chillers:
For packaged RTAC Chillers, it is possible to store the refrigerant in the condenser. It is important to follow the following procedure:
- Ensure that the circuit is turned off.
- Close the liquid line service valve.
- Close the oil return line service valve.
- Start the circuit using the service tool (access the compressor service view in Techview).All fans will be turned on.
- The EXV will open to 100%.
- The oil return line solenoid (if included) will open.
- The unit will start at minimum load.
- The unit will run until it cuts out on low pressure (approximately 6 psia).
- Monitor the suction pressure using a gauge.
- When the unit trips, the discharge check valve will close.
- Close the discharge isolation valve.
- Close the 7/8" oil line shut off valve.
Recover the remaining refrigerant.
Additional details
Notes
- Remote Evaporator ONLY: Because of additional refrigerant piping and charge, the condenser may not be capable of holding the entire charge.
Other Question/Problem/Cause Statements
- Can I do a service pumpdown and store the refrigerant in the condenser?
- How do I do a service pumpdown?
Facts
- Air-Cooled Chiller (Pueblo) (RTAC)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.