How do I drive the expansion valve open with the unit off?
- When the RTAC chiller undergoes a shutdown process, the electronic expansion valve (EXV) is instructed to close.
- To evacuate the line between the EXV and the liquid line angle valve, or to perform a circuit flush following a motor burnout, it is necessary to activate the expansion valve to the open position.
- This can be accomplished by accessing Techview and navigating to Compressor Service View.Within this interface, there are two options available for the EXV: open or auto.
- To fully open the EXV, the auto setting should be selected.
Additional details
Notes
When driving the expansion valve, make sure it is installed into a valve body. If the valve is driven outside of the body, it could cause irreparable damage.
Other Question/Problem/Cause Statements
- How do I drive the expansion valve open with the unit off?
- How can I drive the EXV open to vacuum down the low side?
Facts
- Air-Cooled Chiller (Pueblo) (RTAC)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.