Does the pump output rotate for the chilled water pumps?
CGAM 20-130 Ton
- The pump outputs off of the 1A9 Dual Relay Output will toggle back and forth for each pump when there is a need for a pump to run.
- The CGAM chiller has the ability to start one or two pumps with or without a VFD. For dual pump control without a VFD, the chiller should be configured for Evaporator Pump Control = Dual Pump fixed speed. If configured for Single Pump, only Pump 1 output will be energized.
- When configured for Dual Pump, the CH530 will swap pumps on detection of a fault (if Installed), or when a flow loss or overdue event occurs.
- It will also switch pumps each time the overall pump request is removed and re-engaged, unless a fault is detected on one of the pumps. If faults are detected on both pumps, the unit will be shut down.
- The control will not run both pumps at once.
Additional details
Other Question/Problem/Cause Statements
- Does the pump output rotate for the chilled water pumps?
- How does the pump output work for CGAM chillers?
- Chilled water pump control
- Pump control for CGAM
Facts
- Air-Cooled Chiller (Pueblo) (CGAM 20-130 Ton)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.