During factory testing of units, some discharge line ball valves were found that closed during normal operation of the chiller. The ball valve manufacturer has made a design enhancement to keep the valve from closing during normal operation of the chiller.
The valves are now shipped with a clip that locks the stem in the opened position.
Along with the new clip, a new cap has also been introduced to fit over the clip and properly seal when tightened.
Corrective Action
- All units now ship with the clip installed.
- If a ball valve that closes during normal operation is discovered, install clip and cap to correct the problem.
- See Table 1 for part numbers.
- Obtain the required parts from your local Trane Parts Center.
Parts Ordering Information | Table 1. Parts List
| Part Number | Description | Notes |
|---|---|---|
| CAP01302 | Ball valve cap with clip. | Used on 2-5/8" ball valves. |
| CAP01303 | Ball valve cap with clip. | Used on 1-3/8" ball valves. |
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.
Original HUB Document: DOC-73423