Odyssey Symbio Pairing or Twinning Frequently Asked Questions
Odyssey Pairing or Twinning Limitations and Guidelines
Trane support has had many requests and questions on what kind of equipment can be paired when dealing with Odyssey. There are a few pairings that can cause many difficulties in the field. This document mainly focuses on the issues that arise with the controls wiring and sequence of operation when using Odyssey Symbio products. Refrigerant piping questions should consult the Odyssey piping application guide. Duct design including backdraft dampers for dual air handlers should follow local codes and regulations and follow best practices to prevent excessive external static pressures that may cause air flow issues.
For Odyssey A2L Pairings, there are examples of how to wire the air handler and condenser in the wiring guide, SS-SVN017*-EN. For Odyssey R410A pairings, the wiring guide is SS-SVN016*-EN.
Any other wiring diagrams requests will need to go through the Odyssey Product Manager. They will review the request to determine if there is enough of a business case to allocate engineering resources to create the additional diagrams for this type of pairing.
Product Presale Support and Technical Support do not have the resources to create custom diagrams for every pairing.
Can you twin two air handlers with one condenser?
Pairings that have two air handlers with one dual condenser have caused many issues. If the air handlers are serving two different areas, different heat loads, and/or different thermostats, Symbio controls will not allow this type of application. On legacy and some Reliatel condenser units, you could bring on each circuit independently with a Y1 or Y2. On Symbio controls, however, Y1 or Y2 will bring on the first available stage of cooling (usually this is circuit 1). Of course, this is an issue if you would like to use Y2 to bring on circuit 2 independently. This pairing is not recommended and is not supported.
In some cases where you have two equal size air handlers paralleled in the duct serving the same area with the same thermostat or control, you may could pair the air handlers to one condenser. This type of pairing will require field provided relays to isolate any transformer voltages between the different systems. If you are using a single circuit condenser and manifolding the refrigerant piping from the evaporator coils, you must take care ensure proper oil return to the compressor(s). See the latest Odyssey piping application guide for more information.
The use of Symbio heat pump condensers should be avoided with this application due to issues with electric heat operation in defrost. This is explained more later in this document.
Engineering has reviewed Odyssey A2L twinning of two air handlers and this is not allowed or supported at this time. The complexity of wiring, regulations with the leak detection sensors, and proper leak mitigation control make it potentially hazardous to do this.
Can you twin two condensers with one air handler?
Under no circumstances can two condenser units have the refrigerant piping manifolded or piped together with one refrigerant circuit on an air handler. There is no way to ensure the oil from one compressor will not end up in the other compressor causing eventual and repeat failures.
Two residential condensers can be paired with an Odyssey, dual circuit air handler without much difficulty. The 5 ton Odyssey air handler units already have a transformer installed in them, but any other air handler will need a transformer kit installed. It is recommended an Odyssey TWE 2 Stage Airflow - Symbio use w/ EM, Digit 15 = C or constant volume air handler be utilized for this application. Again, isolation relays will be needed whenever there are multiple transformers used in the system.
Here is an article on a wiring example:
Wiring Odyssey R454B TWE AHU paired with (2) Odyssey TTA Condensers (also contains link for TWA CUs)
Can a single circuit condenser be piped into a dual circuit air handler?
Yes, as long as the refrigerant piping is done according to the recommendations outlined in the Piping Application Guide (Cooling only or Heat Pump).
Can a Symbio Heat Pump be Paired with any unit?
Symbio heat pumps require an Options board to utilize electric heat in defrost mode while in heating operation. Pairing this condenser with legacy air handlers can cause operational issues. The unit will not bring on auxiliary electric heat while in defrost, therefore, the system will be discharging cold air for a short period in the space. In some applications, this may be acceptable, but can cause a dump of cold air on some of the occupants while the unit is supposed to be heating.
Can I pair an Odyssey TWE060 air handler with a residential 5 Ton Condenser?
Yes, you can pair these together. The air handler already has a transformer installed for this type of combination to power the system.
When do I need Communication wire or Purple wire for Symbio?
Communication wire is required for an Odyssey Symbio system when an Options module(s) and/or a VFD programmed for communication is in the air handler. The IMC (intermodule communication) communication allows the Symbio 700 in the condenser to communicate with any Indoor Options Module or Fresh Air Options Module that may be in the air handler. Modbus communication is required for the Symbio 700 to communicate directly to the VFD.
Any SZVAV air handler with the model number 15th digit "D" will need both comm wires ran between the air hander and condenser because it comes with a communication VFD and Indoor Options Module standard from the factory.