Can the chiller start and stop the chilled water pump?
- The chiller does have a pump output which can start and stop the chilled water pump. On the Cold Generator Module (1U48), the Solution Pump output can be found J14-11, 9. This output is tied into 1TB6-6,7; field connections should be made here.
- It is not a requirement that the chiller control the chilled water pump. It should be noted that the programming on the chiller may have to be changed to allow for the fact that the chiller is not controlling the pump.
- For the chiller to control the pump, the operator should access the Setup Menu, select General Unit Functions Setup Submenu, and select "Default Chiller Solution Pump Mode" to AUTO.
Other Question/Problem/Cause Statements:
- Could the chiller start and stop the chilled water pump?
- CGAF Pump Control?
- Pump Control?
- Does the air-cooled scroll chiller have to control the pump?
Additional details
Facts
- Air-Cooled Chiller - Intellipak (CGAC, CGAF)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.