Can the chiller display phase loss and phase reversal diagnostics?
- CG-EB-82 states that these diagnostics will be available when the Current Sensing Module is installed. THIS IS INCORRECT.
- Although this was the intent of the design when the Engineering Bulletin was written, this was never included in the final design.
- In order to detect phase loss or phase reversal, an external phase monitor must be installed and wired to the emergency stop inputs on the chiller (1TB4-16 and 1TB4-17)
Other Question/Problem/Cause Statements:
- Can the chiller display phase loss and phase reversal diagnostics?
- Will the Current Sensing Module allow Phase Loss and Phase Reversal diagnostics to be reported?
- How is Phase loss or Phase reversal detected?
- How is Phase loss or Phase reversal reported?
- What is required to detect and report phase loss or phase reversal?
Additional details
Facts
- Air-Cooled Chiller - Intellipak (CGAC, CGAF)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.