Can a 200 volt chiller be used on a 230 volt power source?
- This is not possible on these chillers.
- These two voltages are out of the +/- 10% voltage utilization range.
- The compressors are built for specific voltage (either 200 volt or 230 volt) application.
Additional details
Facts
- Air-Cooled Chiller - Intellipak (CGAC, CGAF)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.