Is there a Schrader valve on the Low Pressure Cutout switch on CGAE, CGAF, and CGAC chillers?
- As a general rule, schrader valves are to be installed on the low pressure side of scroll chillers under the LPC switch.
- There should be Schrader valves on all the controls except those on the discharge line such as the high pressure cutout.
- Service valves do not have Schrader valves on them independent of their location.
Additional details
Notes
- There will not be schrader valves on the high pressure side of any scroll chiller.
- Caution should be taken to ensure that the Schrader valve is installed when disconnecting a component even when it is supposed to be there.
Facts
- CG series scroll chillers
- Air-Cooled Chiller - Intellipak (CGAC, CGAF, CGAE)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.