Compressors are not at 100% RLA but the maximum capacity output is energized
- Maximum capacity output is energized when the available compressors are at full load.
- Because conditions may be optimum, the compressors may run less than 100% RLA but still be fully loaded up.
- If there is a question whether the chiller is at full load, a tons calculation (tons = (GPM x delta T)/24) should be done to verify the chiller is doing its full load capacity.
- For chilled water loops where glycol is added, a de-rate of capacity should be expected. The sales submittal should be looked at for those conditions.
- Otherwise, for water only loops, refer to the tonnage on the nameplate of the chiller.
Additional details
Facts
- Air-Cooled Chiller (Pueblo) (RTAC)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.