The Hot Gas Bypass (HGBP) option provides a cooling mode with less capacity than that provided by a single stage of compressor cooling. A discharge bypass valve is controlled by a software algorithm that is a timed function (minimum of 10 minutes and maximum of 120 minutes) dictated by the person performing unit setup through the Human Interface.
- With HGBP installed, the unit will always stage up the compressors on circuit 1 first, if operable and stage them down last.
- Hot Gas Bypass is never initiated when staging up compressors (adding capacity), only when staging down.
- If for any reason the last compressor running is not on circuit 1 (circuit 1 is inhibited, or locked out) at the time a subtract command is received, the unit will stage down the last running compressor and bypass the HGBP function.
Additional details
Facts
- Intellipak Air-Cooled Chiller 20-60
- Air-Cooled Chiller (PBL) (CGAD, CGAE)
- Compressor Chiller (PBL) (CCAD, CCAE)
- Water-Cooled Chiller (PBL) (CGWD, CGWE)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.