SUCTION PRESSURE SENSOR FAILURE (CKT-1/CKT-2)
- This diagnostic occurs when there is not a valid signal on the suction pressure sensor input on the SSM (1U91).
- The sensor has an operational range of 0 to 5 VDC.
- These sensors would only exist on units with the Superheat/Subcooling option installed and are located on the suction line of each refrigeration circuit (designated as 4U93 for circuit 1 and 4U95 for circuit 2).
- This is an information only diagnostic and will clear automatically when the module measures a valid voltage.
- This diagnostic will not affect the operation of the unit.
Here are the steps for Intellipak Air-Cooled Chiller
Sensor Calibration Setting
Verify the calibration setting in the pressure transducer device characteristics located in the Setup Menu.
For Suction Pressure Sensors, the settings should be:
0 PSIG = 0.118 VDC & 100 PSIG = 4.847 VDC
The Ckt1 Suction Line Pressure Transducer setup screen appears only if the Superheat/Subcooling option is installed.
This screen allows the user to adjust the voltage to pressure calibration setpoints at 0 PSIG (0.000 - 4.000 VDC) and 100 PSIG (1.000 - 5.000 VDC).
Ckt 1 Suction Line Pressure Transducer
0 PSIG = 0.118 VDC
100 PSIG = 4.847 VDC
The Ckt2 Suction Line Pressure Transducer setup screen appears only on 40-60 Ton units with the Superheat/Subcooling option installed. This screen allows the user to adjust the voltage to pressure calibration setpoints at 0 PSIG (0.000 - 4.000 VDC) and 100 PSIG (1.000 - 5.000 VDC).
Ckt 2 Suction Line Pressure Transducer
0 PSIG = 0.118 VDC
100 PSIG = 4.847 VDC
Wiring Error
Verify the wiring between the Suction Pressure Sensor and the SSM (1U91).
Refer to unit schematics for wire numbers and connections.
If the wiring checks good, proceed to the next step.
Sensor Checkout
- The sensors used to determine suction pressure are 3 wire pressure transducers.
- These transducers require an operating supply voltage of 4.5 ? 5.5 VDC.
- Verify the supply voltage from the SSM (1U91). If the voltage is not in this range, disconnect the plug connector from the SSM (1U91) and verify proper supply voltage.
- If supply voltage is not present, replace the SSM (1U91).
- Once supply voltage has been confirmed, re-connect the plug connector and check the output voltage of the pressure transducer.
- Convert this voltage to a pressure based on the linear scale 0 PSIG (@ 0.118 VDC) to 100 PSIG (@4.847 VDC).
- If the output is not correct versus an actual pressure gauge reading, replace the pressure transducer.
- If the output is not correct versus the HI display of suction pressure, replace the SSM (1U91).
Additional details
Facts
- Intellipak Air-Cooled Chiller 20-60
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.