Symbio UI is a built-in open-source web-based user interface that is used for:
- BAS Configuration
- Viewing alarms
- Configure/retrieve data logs
- Basic setup and configuration of inputs and outputs
- Scheduling
- Alarm Configuration
- Changing unit of measure
- Adjusting airflow (models equipped with ECM fan)
- Manually Testing Outputs
- See Symbio 400B/500: Symbio UI for more info
Tools Required
Computer with a web browser.
Depending on your computer setup, a USB A to B cable or a USB C to B. The B end of the cable connects to the control.
Open a web browser and enter 198.80.18.1 into the address field. Select Log In and follow the prompts.
USB A to B cable
USB C to B cable
WARNING
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.