Overview
BCI-R / BCI2-R Reliatel Fan Control allows users to have full control over the fans in their rooftop units (RTUs). It provides real-time monitoring of the fan speed command, enabling users to optimize the airflow and energy efficiency of the RTU system. Please see below for how to control various BCI-R / BCI2-R Reliatel RTU configurations.
Occupied Operation
Variable Speed Fans (VAV / SZVAV / "Multispeed")
- If RTAM is present, BO/8 will be ignored, and Duct Static will be maintained while occupied
- If no RTAM is present, the fan will operate as follows in occupied mode:
- ACTIVE/TRUE = "Continuous" (Fan will run at minimum speed when load is satisfied)
- INACTIVE/FALSE = "Cycling/Auto" (Fan will turn off when load is satisfied)
Constant Volume / Single Speed Fans:
- ACTIVE/TRUE = "Continuous" (Fan will run constantly when unit is occupied)
- INACTIVE/FALSE = "Cycling/Auto" (Fan will turn off when load is satisfied)
Unoccupied Operation
All Unit Types
- Fan will cycle based on load (unoccupied heat/cool setpoints will be used)
Known/Frequent Issues
- VAV Units: Verify RTAM dip switches 1 and 2 are on/off (you'll need to rebuild points if you have to adjust these dip switches)
- Deadband potentiometer on RTOM is not correct (not controlling to proper duct static) - should be set to 0.2 in H2O
- Cannot manually control variable speed fan from BAS
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.