The TD5 settings for BCI-R / BCI2-R RTU (BAS) Building Automation System control refer to the specific configuration that needs to be applied to the TD5 when a RTU in a BAS application. These setting are crucial in ensuring the the RTU operates efficiently and effectively
- BCI-R / BCI2-R will not go into BAS control. Always remains in Standalone control.
The most likely cause is that a TD5 display is connected and the display is set to 'write mode". It must be changed to "read-only mode" in order for the unit to be put in BAS control.
Configure TD5 Local Display for System Control ("Read Mode")
If a TD5 is present on the unit, by default, it will be configured to be the decision maker for control (aka it's in "Write" mode), and force the unit into "Standalone Operation". In order to enable the RTU to be controlled by the BAS, the TD5 must be in "Read Mode".
1. Settings → 2. Setup → 3. Display Read Only Mode → 4."Read" → 5. Save to display
Additional details
Other Question/Problem/Cause Statements
- BCI-R will not go into BAS control. Always remains in Standalone control.
- BCI-R Binary Output 1 System Control Command shows BAS Control, but Binary Input 1 System Control Status always shows Stand Alone Control
- Tracer TU cannot see the versions or shows incomplete data for the RTAM. RTOM or BCI-R controllers
Facts
- VOYAGER/PRECEDENT BCI-R
- Voyager/Precedent BCI-R
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.