Troubleshoot
| Abbreviation | Abbreviation Name |
|---|---|
| AB | Adapter Board |
| TNS | Transformer |
| CCM | Customer Connection Module |
Does the CCM Module have power?
- Verify that LED 8 is solid green in the middle of the module, and LEDs 5 & 6, located under the P4 connector, are lightly flickering.
- Verify CCM-P5 has 24VAC between Red and Black
- Verify CCM-P5 has 3.2 - 3.9 VDC between Blue and Orange
- If CCM-P5 does not have VAC or VDC, verify that AB-J19 has 24VAC between Red and Black and/or AB-J19 has 3.2-3.9VDC between Blue and Orange.
- If there is no power on AB-J19, verify that AB-J8 is powered between the Blue and Orange wires.
- If there is no power on AB-J8, verify PPF72/PPM72 between the Blue and Orange wires.
- If there is no power on PPF72/PPM72, verify PPF2/PPM2 between the Blue and Orange wires.
- If there is no power on PPF2/PPM2, verify TNS2.
Does the Factory-Installed module have the address plug?
- The Customer Connection Module, when factory-installed, includes an address plug pre-installed on J11. The factory plug is already configured for address 78.
- The rotary dials should be set to 00.
- If the Customer Connection Module says "Not Communicating" on the mobile phone app under Tools > Service, try the steps below.
- If the address plug is securely connected and you have verified the address on the plug, remove the plug and set the rotary dials to 78 (SW1 to 7 and SW2 to 8).
- Cycle power to the unit or reset the IMC link through the mobile phone app. Go to Tools > Service > scroll down to IMC LINK RESET.
Is the Field-Installed module addressed?
- The field-installed Customer Connection Module must be addressed to address 78 on the provided rotary dials.
- SW1 is addressed to 7
- SW2 is addressed to 8
- To verify the communication status, go to Tools > Service on your mobile phone app.
Is the CCM configured?
- To verify the communication status, go to Tools > Service in your mobile phone app.
- When it says Communicating, there should be no active alarms for the Customer Connection Module.
- When it says 'Communicating - Not Configured,' it means the Customer Connection Module is communicating, but there is no configuration associated with it. This will show two active alarms.
- You must configure the CCM under Settings > View Configurations> Edit.
Please click the link below to view the configurations.
- When the Customer Connection Module is not communicating with the Symbio 700 and the unit does not have one, the Symbio 700 configuration is incorrect.
- These points must be verified (Should be set to not installed).
- Remote Minimum Position
- External Auto/Stop
- Ventilation Override
- Alarm Indicator
- Humidistat
- These points must be verified (Should be set to not installed).
Alarms
- Customer Connection Module Communication Status
- Diagnostic: Unit Communication Failure
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.