If the fan speed speed command is set to zero, it means that the fan is effectively turned off
- Fan proving and fan output say on when fan speed is 0% for BCI-R.
- Fan Speed is off but fan output is on.
- MI 41 Supply Fan Status is always On.
- MI 37 Supply Fan Proving Status is always On.
If you have a smaller Reliatel Voyager or Precedent unit (3-25 Ton) the Fan Proving Switch is a normally open circuit. In other words Fan on the input is open, fan off, it is closed. If you do not have the switch, the Supply Fan Proving Status (MI37) always reads ON. The Supply Fan Status (MI41) (it's call Supply Fan Output in Tracer SC) follows the Supply Fan Proving Status. So, it always reports ON, even when the fan is off. The analog input #7 Supply Fan Speed Command will show the true state of the fan command of the Reliatel system.
27.5-50 Ton Reliatel Voyagers have a fan proving switch as standard equipment and it is reversed that of the smaller units. As such, when the fan is off the input is open and when the fan is on the input is closed
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.