With modulating heat, the BCI-R / BCI2-R continuously monitors the temperature in the space and adjust the gas valve's opening accordingly. This ensures that the desired temperature is reached and maintained efficiently.
- How does heat work on BCI-R / BCI2-R RTU with Modulating Heat?
- BCI-R / BCI2-R VAV RTU will not heat
First, make sure your BCI is properly configured for control with an automation system.
In Occupied Heat, duct static pressure is controlled and the Discharge Air Temp (DAT) is controlled to the DAT heating setpoint.
In Supply air tempering, duct static pressure is controlled and the DAT is controlled to the DAT cool setpoint - 3.5 degrees F.
The rooftop will never run occupied heat on its own.
The rooftop has to be commanded to occupied heat to run the occupied heat sequence.
Occupied Heat
Occupancy Request = 1-Occupied
Heat Cool Mode Request BAS = 2-Heat
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.