By performing these control and operational test, the functionality and efficiency of the dehumidification system cam be ensured, resulting in improved indoor air quality and occupant comfort, Additionally, identifying any issues early on allows for timely repairs and prevents major problems down the line.
Under normal operating conditions for the RTU to go into Dehumidification mode, the cooling capacity must be less than 50% and Space Humidity local be greater than the Dehumidification setpoint.
For testing Dehumidification mode for a SCC (Space Comfort Controller) through BAS, it is recommended the "Space Temperature Active" be between the active Heat / Cool setpoints and the "Space Humidity Active" be greater than the "Dehumidification High Limit Setpoint".
Testing the BCI-R ReliaTel Dehumidification operation through a BAS application, requires the BAS application control and manipulate multiple points.
- The below Analog Outputs, Binary Outputs and Multistate Outputs must have the points "out of service" property reset from "true" to "false", when the point are "in service" the BAS value or command will be communicated from the BCI-R to the RTU for control.
- It may take a minute or two, for the RTU and BCI-R to respond to the below setting or adjustments.
Step 1
Verify the following points are in BAS control, as described below:
- BI 1 - System Control Status, BAS control
- MO 7 - Occupancy Request, Occupied / in service
- MO 8 - Heat Cool Mode Request BAS, Auto / in service
- BO 15 - Dehumidification Enable Command, Active = Auto / in service
Step 2
The following points are to put RTU into "Dehumidification" operation:
- AO 2 - Space Temperature Setpoint BAS, 70* / in service
- AO 11 - Space Temperature BAS, 71* / in service
- AO 21 - Space Dehumidification Setpoint BAS, 55% Rh / in service
- AO 25 - Space Humidity BAS, 65% Rh / in service
- AO 29 - Occupied Offset, 3*/ in service
Step 3
The following points to verify "Dehumidification" operation:
- MI 19 - Heat Cool Mode Status / Application Mode Status
- AI 1 - Cooling Capacity Status
- AI 5 - Reheat Capacity Status (if reheat installed)
- AI 11 - Outdoor Air damper Position Status @ Minimum Position
- AI 79 - Dehumidification Capacity Status
Step 4
Reset or Release any points override utilized during Dehumidification operational testing.
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.