There could be several reasons why the BCI-R RTU with WCS Air-FI zone sensor is not bringing on cooling. here are a few troubleshooting steps you can try.
- BCI-R SZVAV with wireless communications will not bring on cooling
- BCI-R SZVAV receiving a communicated space temp BAS will not bring on cooling.
- E-Flex will not bring on cooling
- BCI-R Space Comfort Control (SCC) RTU with wireless communications will not bring on cooling
- BCI-R with Air-FI WCS zone sensor Space Temperature local -40°, stuck in Heat mode
Problem:
BCI-R Space Comfort Control (SCC) with Air-FI WCS has no problem heating or economizing but has problems with mechanical cooling.
Corrective action:
Install a sensor in the return air of the RTU and wire it into RTRM J6, 1-2 terminals.
Could also add a jumper to RTRM J6, 1-2 tells the RTRM the space temp will be communicated.
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.