Oil Flow Control Diagnostic → RTAA 70-125 TON Chillers:
This diagnostic will appear if the compressor model number is set up as CHHB. Because of the different way the control looks at oil flow for the CHHB and CHHN compressor it will disregard the oil flow control for the CHHN thinking it has a CHHB compressor. This can be changed in the Service Settings, Machine Configuration menu, under compressor model number prefix.
- RTAA 130-400 TON → CHHB compressor
- RTAA 70-125 TON, RTUA 70-125 TON, and RTWA 70-125 TON → CHHN compressor
Low oil flow? may have some other valuable information.
In addition it is advised to check the other settings/setpoints in Machine Configuration and Service Setup Menu's.
Additional details
Other Question/Problem/Cause Statements
- Oil Flow Control Diagnostic?
- Oil Flow Control...Circuit 1?
- Oil Flow Control...Circuit 2?
Facts
- Air-Cooled Chiller (Pueblo) (RTAA 70-125 Ton)
- Compressor Chiller (Pueblo) (RTUA)
- Water-Cooled Chiller (Pueblo) (RTWA)
- CHHB compressor IS
- CHHN compressor GP
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.