RTAA, RTWA, RTUA, RTAC, RTHA, RTHB, RTHC, RTHD Chillers:
- RTAA-SB-6B: RTAA, RTWA, and RTUA
- RTAC-SVG02A-EN: RTAC
- RTHA-SB-16: RTHA, RTHB
- No current literature is available for motor burn clean up for RTHC or RTHD chillers
For severe motor burns, there are also outside companies like Refimax or Hudson Technologies that use a refrigerant flush and filtering system. These have been found to be cost effective and provide adequate cleaning.
Additional details
Resource Available
- Reference Literature: (Electronic copies can be pulled from e-library at Trane Residential)
- Service Guide: RTAA-SB-6B, RTAC-SVG02A-EN, and RTHA-SB-16
Other Question/Problem/Cause Statements
- Motor Burn Cleanup Procedures?
- What are the motor burn clean-up procedures?
- How do I clean up the chiller after a motor burn?
- Motor Burn. Is there a bulletin that shows replacement procedure?
Facts
- Air-Cooled Chiller (Pueblo) (RTAA 70-125 Ton)
- Air-Cooled Chiller (Pueblo) (RTAA 130-400 Ton)
- Air-Cooled Chiller (Pueblo) (RTAC)
- Water-Cooled Chiller (Pueblo) (RTHA)
- Water-Cooled Chiller (Pueblo) (RTHB)
- Water-Cooled Chiller (Pueblo) (RTWA)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.