Is the CGAM expansion tank ASME certified?
The CGAM chiller will ship standard with an expansion tank when the factory installed pump package option is selected. The buffer tank is optional.
Both the expansion tank and the buffer tank fall outside the scope of ASME Boiler and Pressure Vessel Code Section VIII. ASME only requires certification on vessels containing water if the design pressure exceeds 300 psi (2MPa). If the design pressure is less than 300 psi, it is outside the scope of the code.
The CGAM pump package, expansion tank and buffer tank will have a maximum working pressure of 150 psig.
See the attachement below for an excerpt from the ASME Boiler and Pressure Vessel Code Section VIII scope.
Additional details
Other Question/Problem/Cause Statements
- Is the CGAM expansion tank ASME certified?
- Is there a U-1 report for the expansion tank?
- Does the expansion tank meet the ASME Pressure Vessel Code Section VIII?
- Is the CGAM buffer tank ASME certified?
- Is there a U-1 report for the buffer tank?
Facts
- Air-Cooled Chiller (Pueblo) (CGAM 20-130 Ton)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.