There are 3 options of Liquid level sensors in the options setup menu. Make the appropriate selection based on the sensors installed on the unit.
The one with the “Level Sensor with Integrated Electronics” in the description needs to be selected if you have the 56MM sensor.
In some cases the liquid level sensors must be upgraded to be used in AdaptiView. First try binding the way they are. If they bind, no further action is required. If they will not bind, they will show up as extra LLIDs. Unbind these and rebind. During rebinding update the LLID firmware when prompted. Do these one at a time. May have to go through the unbind/rebind process a second time after upgrading. Follow the attached screenshots and instructions if necessary.
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.