- Connect to Symbio 700 with Tracer TU via USB or SC+/Synchrony connection.
Select the TOOLS drop-down and select RETRIEVE DATA LOGS.
In the Retrieve Data Logs window, select the desired data logs and hit RETRIEVE.
- Once the process has begun, the Progress for each data log will update one at a time.
- Once status on all selected data logs shows Done, select Close.
- To access the retrieved data logs, access Documents\Tracer TU\Data Logs\Symbio 700\<select controller type-Odyssey/Precedent/Voyager III>
- Each data log will be present as an individual .csv file .
At this time, neither Symbio 700 or Tracer TU combine data logs into one large file.
Data logs for all like equipment types are stored in the same folder, data logs from two separate units will store in the same folder, recommend pulling each unit's files into a job folder before starting the next data log collection.
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.