Table of Contents
Symbio 700 Data Log Information
- Symbio 700 by default data logs many crucial points by itself, but can also have more data logs added using Tracer TU.
- The default data logs sample every 10 seconds for 50,000 samples providing 5.89 days of data
- The Symbio platform exports data logs as individual *.csv files that can be viewed individually using Microsoft Excel or any program that can open *.csv files.
- Unfortunately, the Symbio platform does not combine the files as one large file on export.
Do you have access to Tracer TU → Symbio™ 700 - Retrieving Data Logs with Tracer TU
Retrieving Data Logs with the Symbio App
- Connect a USB thumb drive in the USB port on the top left of the Symbio 700
- Flash drive must be 1GB or larger and using FAT32 file format
- Connect to Symbio 700 with Symbio Service & Installation Mobile App using Bluetooth.
- Click this link for instructions on how to connect → Symbio™ 700 - Bluetooth Connection Instructions
- Navigate to TOOLS>EXPORT DATA LOGS:
- Select "Export Data Logs"
- Symbio 700 will start exporting the data logs to the USB, do not power down the controller and allow the app to finish before navigating away.
- Note: Symbio 700 will continue to operate as normal in the background.
- The app will alert when the data log export is complete
- Once the logs are on the USB, they can be viewed with Microsoft Excel or any application that allows viewing of *.csv files.
- Symbio does produce a separate file for every data logged point.
Viewing Data Logs on the Symbio App
- Connect to Symbio 700 with Symbio Service & Installation Mobile App using Bluetooth.
- Click this link for instructions on how to connect → Symbio™ 700 - Bluetooth Connection Instructions
- Navigate to TOOLS>VIEW DATA LOGS:
- Select the desired data logs to view from the list (up to 4 logs) and select "View Multiple":
- The app will display the selected logs over the first day of the available data
- The user can the time frame and day by selecting the blue text at the top of the screen:
- Then you can narrow the time frame of the day:
- Then the user can select what day and what time (set day first then app will prompt for what time):
- Clicking the data points on the screen will show the value of that point