Make sure the app is installed on your phone (see "Where to Get the Symbio 700 Phone App"). After installing the app and connecting to the device (see: "Bluetooth Connection Instructions", follow these steps below to change the BACnet/IP.
Video
Phone App Procedure
Step 1
Connect with the Phone App. Once you're on the homepage, click Tools.
Step 2
Select Protocol Configuration.
Step 3
Press Edit on the upper right-hand side of your phone.
Step 4
Change by touching the dropdown arrow at Protocol (Image 1). Change it from BACnet MS/TP to BACnet/IP. In this part of the menu, this is where the network number, UDP port, and BBMD can be changed after BACnet/IP is selected and saved. It should look like Image 2 below. Once the changes have been made, Save your changes.
Once the configuration has been changed to BACnet/IP, you can open IP Configuration to change the IP address to Static IP. If DHCP is required, it is set up as the default.
Step 1
Select IP Configuration
Step 2
Select the Edit button to configure all changeable settings.
Step 3
Change the IP address to a static IP address. Click DHCP, then select Static (step 3A).
-
Change to Static IP Address
-
Once the Static IP Address is selected, it can be changed to the required IP address, Subnet Mask, and Gateway.
Step 4
Changing the DNS from automatic to Static DNS
-
Change to Manual DNS
-
On the edit screen, the DNS can be manually changed. Once the Changes have been made, Save your changes then.
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.