BCI-R points need to be configured very specifically for BAS control
- You will need to control the "Active Value" and "Out of Service" BACnet properties with one of the following tools
- Tracer TU
- Trane BACnet Setup Tool - BACnet Setup Tool - Setup UC/BCI for Integration into BAS
-
BACnet Building Automation System / Front End
- Unit should operate correctly in ReliaTel Test Mode before beginning.
Process
1. Configure necessary/relevant BCI-R / BCI2-R Points for System / BAS Control (required for any BAS control)
MANDATORY Point Settings for System / BAS control
- You will be configuring the 1. "Out of Service" and 2. "Present Value" BACnet properties for the following points to get the unit running with a building automation system. The majority of the points below are created "Out of Service"; (aka Out of Service = ACTIVE/TRUE). You will need to make them "In Service" (aka Out of Service = INACTIVE / FALSE).
-
TD5 operator display must be set to "Read" mode: LCU-BCI-R-TD5-Settings-for-RTU-BAS-Control
Table 1: Mandatory settings
Point Type / InstancePoint Name 1. "Out of Service" BACnet Property 2. Present Value
(BACnet Property)Notes 1 BO/1 System Control Command FALSE (aka "In Service") ACTIVE ("BAS Control") 2 BO/8 Supply Fan Configuration Command FALSE - ACTIVE ("Continuous")
- INACTIVE ("Cycling / Auto")
3 BO/13 Filter Timer Reset FALSE INACTIVE 4 BO/14 Diagnostic Reset Command FALSE INACTIVE 5 MO/7 Occupancy Request FALSE 1-Occupied
2-Unoccupied
6 MO/8 Heat Cool Mode Request BAS FALSE 1-Auto
5-Cool
7 BI/1 System Control Status FALSE not writeable
-
2. Optional System Control Settings and Troubleshooting
Fan & Duct Static Pressure Control
If an RTAM board is present, unit will control to duct static when occupied and BO/8 will be ignored
Otherwise, when in service, BO/8 dictates your occupied fan operation.
For unoccupied operation and more details:
Space and Discharge Air Control
For your BAS to control space temperature, setpoint limits, discharge air temp and duct pressure:
Mechanical Cooling
- E-Flex Unit Operation and Troubleshooting
- Standard Compressor
Heating Control
Frequent source of issues, especially VAV units with staged heat
- VAV Units
- CV & SZVAV Units
- Present Value MO/8 (Heat Cool Mode Request) = 2-Heat (still working on confirming this and any exceptions)
- Present Value MO/8 (Heat Cool Mode Request) = 2-Heat (still working on confirming this and any exceptions)
Outdoor Air - Economizing, Demand Control Ventilation (more coming soon)
- LCU BCI-R RTU - Outdoor Air Control; Economizer & Ventilation
-
LCU BCI-R Unit does not respond to rise in CO2 level. How does Demand Control Ventilation work on the BCI-R
Dehumidification (in development)
Diagnostics and other troubleshooting
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.