Entering Evaporator Water Temperature
- Pueblo built evaporators are designed for a maximum entering water temperature of 108 deg F (42 C). Temperatures above 108 can cause warping of the polypropylene baffles in DX evaporators (RTAA, RTWA, RTUA, CGWD, CCAD, and EVP) and temperatures above 130 deg F (54 C) can cause relief valves to "lift".
- CGAM, ACSA, ACX Maximum temperature is 125 deg F (52 C).
- RTAE, ACRA, ACRB, RTAC, and RTAF Maximum entering water temperature is 108F (42 C) for initial water temp for pull down. It is also the maximum temperature for water running through the evaporator when the chiller is off. Maximum entering water temperature for stable operation should not be higher than 88F (68F + 20F).
Pueblo Air-Cooled Chillers:
The easiest way to determine is by running a selection in TOPSS, based on leaving water temperature AND minimum flow rate for the chiller selected. The output will show the maximum entering water temperature.
Water temperatures exceeding these values can cause relief valves to open.
- Maximum water temperature unit off
- CGAM - 125°F
- ACS/ACX - 125°F
- ACR/RTAC/E/F - 108°F
- RTAA/RTWA/RTUA/CGWD/CCAD - 108°F
- Temperatures above 108 can cause warping of the polypropylene baffles in DX evaporators
- Maximum water temperature start up
- CGAM - 125°F
- ACS/ACX - 125°F
- ACR/RTAC/E/F - 108°F
- Maximum water temperature sustained
- 90°F for all air-cooled chillers
Notes
- See RLC-DS-2 for reference.
Additional details
Other Question/Problem/Cause Statements
- Entering Evaporator Water Temperature
- Warmest water evaporator can handle
- What is the hottest water that can run through the evaporator?
- Evaporator limitations
- Maximum water temperature allowed in evaporator while unit is not operating
- Switching over from heating, at what temperature can chiller be enabled?
- Thermal stress limit
Facts
- Air-Cooled Chiller (Pueblo) (RTAA 130-400 Ton)
- Air-Cooled Chiller (Pueblo) (RTAA 70-125 Ton)
- Air-Cooled Chiller (Pueblo) (RTAC)
- Compressor Chiller (Pueblo) (RTUA)
- Evaporator Chiller (EVP)
- Water-Cooled Chiller (Pueblo) (RTHC)
- Water-Cooled Chiller (Pueblo) (RTWA)
- Water-Cooled Chiller (Pueblo) (RTHB)
- Water-Cooled Chiller (Pueblo) (RTHD)
- 2 pipe system (heating & cooling)
- Air-Cooled Chiller (Pueblo) (CGAM 20-130 Ton)
- Air-Cooled Chiller - Intellipak (CGAF)
- Compressor Chiller (Pueblo) (CCAF)
- Compressor Chiller (Pueblo) (RTUD 70-200 Ton)
- Water-Cooled Chiller (Pueblo) (CGWF)
- Air-Cooled Chiller (Pueblo) (RTAE)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.