This diagnostic is an indication that the CLD is experiencing issues communicating with the Chiller Module (1U1).
To determine which module(s) to replace, the technician should follow this procedure:
- Check communication wires between Chiller and CLD.
- Unplug all other communication wires except for CLD and Chiller Module If problem goes away, add additional modules back on to the communication link until the problem reoccurs to determine which module (or wire) is causing problems.
- If the problem persists with only the CLD and the Chiller Module connected, the 1U1 Chiller Module should be replaced first.
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.