Dynaview replacement process for RTAC units ONLY
Dynaview Replacement is attached below. Open it to view the steps described below
TechView screen (non-Trane technicians)
KestrelView screen (Trane technicians)
- Before you remove the damaged DV (Dynaview) from the unit, connect to it with KestrelView (Techview).
Go to “Unit View” Record the Starts and Hours of each one of the compressors.
- It is recommended to also go to Configuration → Nameplate tab, Record the Model Number and Confirm Code and compare to the unit nameplateNameplate will be based on the configuration from the factory.
The values within Configuration → Nameplate tab includes all changes to the configuration since the unit was shipped from the factory. Generally, it is recommended to used these values rather than nameplate.
- It is recommended to also go to Configuration → Nameplate tab, Record the Model Number and Confirm Code and compare to the unit nameplateNameplate will be based on the configuration from the factory.
- Remove power from the chiller.
- Remove and replace faulty Dynaview.
- Reapply power to the chiller.
- Perform a Techview local connection.
- Message indicating "No Application Present" will be displayed.
- Follow the prompts.
Select the product type: RTA
- Next select the highest available MP firmware version.
- Select Download Software to Main Processor.
- The software will load, then you will be prompted to configure the chiller.
- RTAC units will use the model number, serial number, and confirmation code (CRC) to load configuration.
- This numbers can all be found on the unit nameplate or the values recorded in previous step.
- These values must be loaded into the "NAMEPLATE" tab within the Configuration menu.
For an example of the process, use the link above.
- RTAC units will use the model number, serial number, and confirmation code (CRC) to load configuration.
Once the configuration has been loaded by one of the previous methods, select LOAD CONFIGURATION at the bottom of the screen to compete the download to the CH530.
- Update the following details:
- Chilled water setpoint.
- Differential to start and stop.
- Compressor starts and hours.
- Must be completed using KestrelView in Access Level 4.
- Leaving water temperature and low refrigerant temperature cutout values (based on water-only or glycol).
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.