Is it ok to mount the paddle-style condenser water flow switch downstream of the condenser water regulating valve?
It is best to follow the manufacturer's guidelines for the best installation.
- The flow switch should be located in a horizontal section of pipe where there is a straight horizontal run of at least 5 pipe diameters on each side of the flow switch. The flow switch may be installed in a vertical pipe if the flow is in the upward direction.
- The flow switch must be installed in the upright position as shown with arrow mark on side of casting in the same direction as fluid will flow.
- Some system conditions that require more than 5 pipe diameters are high viscosity fluid and high fluid velocity.
- The flow switch must be installed in the pump suction piping when spring-loaded check valves and/or other close coupled accessories are installed in the pump discharge piping.
Text from the diagram below:
- 1" PIPE CONNECTION
- FLUID FLOW
- 5 x D MINIMUM
- D = PIPE DIAMETER
Additional details
Other Question/Problem/Cause Statements
- Is it ok to mount the paddle-style condenser water flow switch downstream of the condenser water regulating valve?
- Are there any recommendations for installing a paddle-style condenser flow switch?
- Paddle-style flow switch mounting?
Facts
- RTHD
- Air-Cooled Chiller - Intellipak (CGAF)
- Air-Cooled Chiller (CGA, 10-15 Ton)
- Air-Cooled Chiller (PBL) (CGAD, CGAE)
- Compressor Chiller (PBL) (CCAD, CCAE)
- Compressor Chiller (Pueblo) (CCAF)
- Compressor Chiller (Pueblo) (RTUA)
- Water-Cooled Chiller (PBL) (CGWD, CGWE)
- Water-Cooled Chiller (Pueblo) (CGWF)
- Water-Cooled Chiller (Pueblo) (RTHA)
- Water-Cooled Chiller (Pueblo) (RTHB)
- Water-Cooled Chiller (Pueblo) (RTHC)
- Water-Cooled Chiller (Pueblo) (RTHD)
- Water-Cooled Chiller (Pueblo) (RTWA)
- Water-Cooled Chiller (Pueblo) (RTWD)
- Air-Cooled Chiller (Pueblo) (RTAA 130-400 Ton)
- Air-Cooled Chiller (Pueblo) (RTAA 70-125 Ton)
- Air-Cooled Chiller (Pueblo) (RTAC)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.