Issue:
Unit Paint Color
Resolution:
Pueblo uses 2 colors of paint in our Chillers:
RTHA, RTHB, RTHC, RTHD, RTWD, RTWA, RTUA, CGWF, and CCAF are all completely painted with Executive Beige paint.
The RTAA, RTAC, RTCA, CGAM, CGAF, RTAE, ACR, ACX, and ACS are Slate Gray.
Note, because the panels of RTAA, RTAC, RTCA, RTAE, RTAF, ACR, ACX, and ACS are finished using a "powder coat" process, spray painting rarely produces a perfect match.
Air-cooled touch up paint:
Slate Grey
PAI00077 1 gallon
PAI00086 12 oz spray
Water-cooled touch up paint:
Executive beige
PAI00061 12 oz spray
PAI00062 1 gal
Touch-up paint can be purchased at the local Trane Parts Center.
Air-cooled powder coat paint:
Paint Brand: Tiger Drylack
Paint color #: 249/70490
Paint color: Slate Gray
Air-cooled 2 part water based epoxy paint:
Paint Supplier Colorado Paint
Paint number: MF502BSG
Paint color: Slate gray
Paint Supplier Colorado Paint
Paint number: MF502
Paint color: Trane epoxy Resin A Clear
Water-cooled water based acrylic enamel paint:
Paint Brand: EvoTech Industrial Coatings
Paint number: 522214
Paint Color: Trane Beige
Notes:
Contact product support if MSDS sheets are needed for chiller paint.
Resource Available:
-
Tech TV Video(s):
- N/A
-
Reference Literature: (Electronic copies can be pulled from e-library at Trane Residential (tranetechnologies.com))
- IOM:
- Service Guide:
-
Other:
- PART-SVB17C-EN and ElectroFin Touch-up Paint
Changes:
Other Question/Problem/Cause Statements:
- Unit Paint Color
- What is the color of the paint on the chiller?
- What color of paint is used on Pueblo built chillers?
- What is the part number for paint of the chiller?
Facts:
- Air-Cooled Condenser (RTCA)
- Air-Cooled Chiller (Pueblo) (RTAA 130-400 Ton)
- Air-Cooled Chiller (Pueblo) (RTAA 70-125 Ton)
- Air-Cooled Chiller (Pueblo) (RTAC)
- Air-Cooled Condenser (Pueblo) (RTCA)
- Compressor Chiller (Pueblo) (RTUA)
- Water-Cooled Chiller (Pueblo) (RTHC)
- Water-Cooled Chiller (Pueblo) (RTHD)
- Water-Cooled Chiller (Pueblo) (RTWA)
- Water-Cooled Chiller (Pueblo) (RTHB)
- Compressor Chiller (Pueblo) (CCAF)
- Water-Cooled Chiller (Pueblo) (CGWF)
- Water-Cooled Chiller (Pueblo) (RTWD)
- Air-Cooled Chiller (Pueblo) (CGAM 20-130 Ton)
- Air-Cooled Chiller (Pueblo) (RTAE)
- Air-Cooled Chiller (Pueblo) (ACRA)
- Air-Cooled Chiller (Pueblo) (ACSA)
Document Identifier: DOC-79282
Document Identifier: 79282
Click the e-library symbol for the latest version
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.