Can temperature sensor wires be cut?
- The connections at the modules are done with Amp MTA connectors and those are best made with a special tool.
- If the service technician cuts the cable, it is important to end up with the spliced connection inside the cabinet.
- The splice should never be made with wire nuts or butt splices.
- The wires must be cleaned bright and soldered with rosin core solder.
- Shrink-wrap should be applied over the splice.
Additional details
Other Question/Problem/Cause Statements
- Can temperature sensor wires be cut?
- Replacing the sensors
- Sensor replacement procedure
Facts
- Air-Cooled Chiller - Intellipak (CGAC, CGAF)
- Air-Cooled Chiller (CGA, 10-15 Ton)
- Air-Cooled Chiller (Pueblo) (RTAA 130-400 Ton)
- Air-Cooled Chiller (Pueblo) (RTAA 70-125 Ton)
- Air-Cooled Chiller (Pueblo) (RTAC)
- Air-Cooled Condenser (Pueblo) (RTCA)
- Compressor Chiller (Pueblo) (RTUA)
- Water-Cooled Chiller (PBL) (CGWA, CGWB, CGWC, CCAA, CCAB, CCAC)
- Water-Cooled Chiller (PBL) (CGWD, CGWE, CGAD, CGAE, CCAD, CCAE)
- Water-Cooled Chiller (Pueblo) (CGWF, CCAF)
- Water-Cooled Chiller (Pueblo) (RTHA)
- Water-Cooled Chiller (Pueblo) (RTHB)
- Water-Cooled Chiller (Pueblo) (RTHC)
- Water-Cooled Chiller (Pueblo) (RTHD)
- Water-Cooled Chiller (Pueblo) (RTWA)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.