Display is locked up and the keys do not work.
RTAA, RTWA, RTUA
- Check the four LED's on the CLD Module (Display or 1U6).
- The ST LED should be on continuously...if it blinks it indicates the processor is repeatedly being reset.
- The +5V Dc LED should also be on continuously. It will go out if power drops below normal operating voltage.
- The TX LED should blink every second or two as the 1U6 transmits on the IPC link.
- The RX LED should blink continuously, indicating that other modules are communicating.
- The display communicates with the Chiller Module (1U1) via a twisted IPC link.
- The link originates on TB1 -1 of the 1U6 and then goes to the P11 connector on the 1U1. From there it daisy chains to the other modules.
- Try to isolate just the 1U1 and the 1U6 on the buss by removing the P51, P41, P31 and P21 (options module may not be present) connectors. If the keys are functional, bring on the modules one at a time until the suspect board is found.
- Inspect the display for signs of moisture that may have corroded the display. If noticeable corrosion is present, try cleaning printed circuit board with isopropyl alcohol.
- Check TP voltages on the Chiller Module.
Notes
- Refer to troubleshooting service bulletin RLC-SVD03A-EN for detailed procedures.
Additional details
Other Question/Problem/Cause Statements
- Display is locked up and the keys do not work.
Facts
- RTAA 70-125 TON (PUEBLO)
- Air-Cooled Chiller (Pueblo) (RTAA 70-125 Ton)
- Compressor Chiller (Pueblo) (RTUA)
- Water-Cooled Chiller (Pueblo) (RTWA)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.