What size wire do I need to pull for the chiller?
RTAC, RTAA, RTUA, RTWA, CGWF, CCAF, RTHB, RTHC, RTHD, CGAM, RTAF, RTAE
- Chillers may be purchased with either Main Terminal Block, Disconnect or Circuit Breaker.
- The lug size on the respective component will accept a certain wire size and the number of poles per phase.
- The catalog and IOM might not have the most current data, so the most accurate document which will have the correct information is always listed on the submittal.
- Refer to it to determine which size wire size and the number of wires that should be used/pulled.
- Wire range size per lug information is included in the dimensional drawings exportable from TOPSS. (see attachment below for visual reference)
- Refer to NEC 440-33 for wire sizing and ampacity.
Additional details
Other Question/Problem/Cause Statements
- What size wire do I need to pull for the chiller?
- Ampacity
- Wire size?
- Power wire size?
- Where can I find the wire sizes the chiller will accept?
- What size wires will the lug accept?
Facts
- Air-Cooled Chiller (Pueblo) (RTAA 70-125 Ton)
- Air-Cooled Chiller (Pueblo) (RTAC)
- Compressor Chiller (Pueblo) (RTUA)
- Water-Cooled Chiller (Pueblo) (RTHB)
- Water-Cooled Chiller (Pueblo) (RTHC)
- Water-Cooled Chiller (Pueblo) (RTHD)
- Water-Cooled Chiller (Pueblo) (RTWA)
- Air-Cooled Chiller (Pueblo) (CGAM 20-130 Ton)
- Air-Cooled Chiller (Pueblo) (RTAE)
- Air-Cooled Chiller (Pueblo) (RTAF)
- Compressor Chiller (Pueblo) (CCAF)
- Compressor Chiller (Pueblo) (RTUD 70-200 Ton)
- Water-Cooled Chiller (Pueblo) (CGWF)
- Water-Cooled Chiller (Pueblo) (RTWD)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.