In which orientation are the isolators placed underneath base rail?
- Isolators should be oriented with the widest side perpendicular to the base rail in order for the mounting slots to be accessible.
- Secure the isolators to the mounting surface using the mounting slots in the isolator base plate. Do not fully tighten the isolator mounting bolts at this time.
- Align the mounting holes in the base of the unit with the threaded positioning pins on the top of the isolators.
- Lower the unit on to the isolators and secure the isolators to the unit with a nut.
- Level the unit within a 1/4" length and width (refer to submittal and IOM).
- Fully tighten the isolator mounting bolt.
The "ears" of the isolators that stick out past the rail will have a metal plate inside the rubber to allow for the bolts to tighten.
For installations where the "ears" will be floating over the edge of a rail/beam, a metal plate could be welded to the beam to support the entire isolator.
Additional details
Other Question/Problem/Cause Statements
- In which orientation are the isolators placed underneath base rail?
Facts
- Air-Cooled Chiller (Pueblo) (CGAM 20-130 Ton)
- Air-Cooled Chiller (Pueblo) (RTAC 140-500 Ton)
- Air-Cooled Chiller (Pueblo) (RTAF 115-520 Ton)
- Air-Cooled Chiller (Pueblo) (RTAE 150-300 Ton)
- Air-Cooled Chiller (Pueblo) (ACSA 140-230 Ton)
- Air-Cooled Chiller (Pueblo) (ACRA 150-300 Ton)
- Air-Cooled Chiller (Pueblo) (RTWD 60-250 Ton)
- Air-Cooled Chiller (Pueblo) (RTUD 80-250 Ton)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.