LLID control module is being damaged when the EXV motor windings are shorted.
- If you have a LLID control module that has been damaged when plugging it into the EXV motor it could be a short in the motor winding resistance.
- The following winding resistance check will determine if you have a bad EXV motor.
- Perform this check prior to replacing the LLID control module otherwise you will damage the new LLID.
Checkout Procedure:
- Using an Ohmmeter, perform the following steps
- Each coil should be approximately 75-100 ohms on opposite pins
- Adjacent pins must read OPEN
- Pins to valve body must read OPEN
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.