Does a chiller wired in with no branch circuit protection meet proper codes and installation requirements?
This is not allowed per NEC 440-III and most local codes have adopted this as part of their local code requirements.
Additionally, by applying a UL sticker to the Trane chiller, it is understood and approved by UL that its requirements are met for internal chiller wiring protection as long as the branch circuit is protected.
Additional details
Other Question/Problem/Cause Statements
- Does a chiller wired in with no branch circuit protection meet proper codes and installation requirements?
Facts
- Air-Cooled Chiller (CGA, 10-15 Ton)
- Air-Cooled Chiller (CGAA)
- Air-Cooled Chiller (Pueblo) (RTAA 130-400 Ton)
- Air-Cooled Chiller (Pueblo) (RTAA 70-125 Ton)
- Air-Cooled Chiller (Pueblo) (RTAC)
- Air-Cooled Condenser (Pueblo) (RTCA)
- Compressor Chiller (Pueblo) (RTUA)
- Water-Cooled Chiller (Pueblo) (RTHA)
- Water-Cooled Chiller (Pueblo) (RTHB)
- Water-Cooled Chiller (Pueblo) (RTHC)
- Water-Cooled Chiller (Pueblo) (RTHD)
- Water-Cooled Chiller (Pueblo) (RTWA)
- Water-Cooled Condensing Unit (RWUD)
- Air-Cooled Chiller (Pueblo) (CGAM 20-130 Ton)
- Air-Cooled Chiller (Pueblo) (RTAE)
- Compressor Chiller (Pueblo) (CCAF)
- Water-Cooled Chiller (Pueblo) (CGWF)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.