When mineral oil is found in Pueblo built 134a chillers is found, the following cleanup procedure can be used to clean system:
The mineral oil when used in R134a is not miscible. The mineral oil will turn to a thick wax-like substance that floats on the liquid in the evaporator and coats the tubes with a layer of wax. You will need to use a solvent to dissolve the mineral oil.
- Connect a drum of the R22 to the bottom of the chiller and fill the shells with liquid R22 using a transfer pump.
- Vent the vapor back to the drum.
- Drain the refrigerant (contaminated with mineral oil) from the shells. This flushing procedure will dissolve the wax and allowing it to be removed from the shells.
- Run the contaminated R22 through a distilling process to separate out the mineral oil.You will need to do this for both shells and you will need to somehow flush the interconnecting lines and internal surfaces of the compressor as well
- To accomplish this could take a large amount of liquid, perhaps 3 times the normal system charge
- If you have isolation valves that will help
- As an alternate, if you can get your hands on some R12, it will work equally good in dissolving the oil.
- You could even run the RTHC/RTAC for a couple hours to flush the I/C pipes and the compressor
- A second alternative would be to charge the chiller with R22 and run it for a couple of hours, while being careful to keep condensing pressures below 200 psig
- Both of these approaches would reduce the amount of R22 required to flush the system and would be more effective in getting the mineral oil out
- You will probably need to do this at least twice
Our experience has been that the residual of mineral oil left in the system must drop to 1%, or less. A chemical sample should be taken of the R22 that has been withdrawn to see how contaminated with mineral oil it is after each flushing procedure.
Additional details
Other Question/Problem/Cause Statements
- Mineral Oil Contamination in 134a Chillers
Facts
- RTAC
- RTHC (Pueblo)
- RTHD
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.